Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

Damping Function in response simulation

Hi every body,

 

I have Damping function i.e a list of frequencies along with the damping values got from the model testing. this data i want to give as an damping input during the response simulation nx. insted of using the constant viscous damping for all the frequencies.

for example i have 

 

20Hz 0.05 damping

552Hz 0.02damping

980hz 0.012 damping

 

help me in this 

 

karthik

3 REPLIES
Solution
Solution
Accepted by Ganesh_S (Community Manager)
‎08-26-2015 04:32 AM

Re: Damping Function in response simulation

Karthik,

 

Response Simulation supports modal damping as you describe. After creating a response simulation, the navigator will have an item for the underlying solution's normal modes. There are a couple ways to define modal damping from there.

 

1. Select the normal modes item and MB3 Edit Damping Factor

2. From the same menu, use the Rayleigh's damping feature to compute modal damping values

3. Same menu again, edit damping scale factors - leaves the existing damping settings alone, but scales them during results processing.

 

You can define individual modal damping factors too via the Response Simulation Details View portion of the Simulation Navigator.

 

1. Select the normal modes item as mentioned above

2. Expand the Response Simulation Details View

3. Select any mode and MB3 Edit Damping Factor

 

The attached JPG shows where in the navigator you go to define modal damping properties.

 

Regards,

Mark

 

Mark Lamping

Simulation Product Management

Product Engineering Software

 

Siemens Industry Sector

Siemens Product Lifecycle Management Software Inc.

Mark.Lamping@siemens.com

Re: Damping Function in response simulation

Thak you sir

as per your sugetion the problem of mineis solved.

i have one clarification.

i want to give a contant resolution of 5Hz for solving the response analysis.

there is a option in NX to give even, log-log but there there is no place where i can give the dt values.

plz breaf me.

 

For example i want to get the respone at every 5Hz interval i.e (from 20Hz- 2000Hz i should have 396 points).

 

Thank you.

Re: Damping Function in response simulation

Sir 

is any body is having the solution for this .

 

Thankyou.