Cancel
Showing results for 
Search instead for 
Did you mean: 

Direction dialog in the force window is gone

Pioneer
Pioneer

Hello,

 

I am using NX9, version 9.0.3 MP06. For a while now I am missing the dialog for the force direction. I know that the availible boundary conditions depent on the solver selected, but I am doing just a simple 101 linear thing. When I want to define a force, I can not define its direction any more. When I open the same file with NX10 the dialog is complete?

 

force_direction_gone.PNG

 

For this time I can use the "normal" option and negative forces as workaround, but still, where is the dialog?

 

Any sugesstions?

 

JonkMcCool

2 REPLIES

Re: Direction dialog in the force window is gone

Siemens Phenom Siemens Phenom
Siemens Phenom

You've got the dialog in a custom state. RMB on the Dialog Options button in the extreme upper left corner. Use "Show Collapsed Groups" and/or Force(more) to enable all of the groups.

 

Custom state:

 

Force_Custom.png

 

Full state:

 

Force_All.png

Re: Direction dialog in the force window is gone

Pioneer
Pioneer

Thank you,

 

I don't know why it was hidden in my settings. In my oppinion the option "direction" should not be able to be hidden in a dialog that is called "direction and magnitude" in the first place. But that is only my point of view :-)

 

Anyhow, thank you for your help!

 

JonkMcCool