Cancel
Showing results for 
Search instead for 
Did you mean: 

Edge to Surfaca Contact

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello,

 

Is there an option to define edge to surface contact for shell meshes (imagine a T like contact situation) ? You have this option for GLUE, but as I see NX Nastran does not offer such contact option.

 

Thanks

 

Akgun

4 REPLIES

Re: Edge to Surfaca Contact

Siemens Phenom Siemens Phenom
Siemens Phenom

You are correct in the context of edge-surface glue not having a general contact equivalent. Edge-edge contact exists, but that assumes that the 2D elements are very close to being in the same plane. There is a general surface-surface contact too, but that doesn't apply to your situation.

 

SOL 601 advanced non-linear does support node to surface contact. Don't take my word for it that it solves your problem, but I think it is worth reviewing the documentation and testing if it sounds promising. I believe you can set this up as surface to surface contact, but the source side is really reduced to nodes. Your edge elements would be the source in a surface to surface contact pair. Or maybe a better NX Nastran user can confirm that it can properly model shell edge to surface contact with its node to surface contact capabilities.

 

Regards,

Mark

Re: Edge to Surfaca Contact

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thank you Mark, let me review and try this, then I will let you know the outcome.

 

Akgün

Re: Edge to Surfaca Contact

Experimenter
Experimenter

Hello Akgün

 

I have a similar problem as you had. In the surface to surface contact I chose the edge as source and the shell below as target, but the contact doesnt work.

Did you find a solution?

 

kind regards 

onon

 

Re: Edge to Surfaca Contact

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

 

In my case I continued to use edge to surface GLUE using SOL 401, nonlinear material properties were priority for me. However as I see from your picture you have to use contact.

 

You can maybe try new SOL 402.

 

AK