Cancel
Showing results for 
Search instead for 
Did you mean: 

Export max group temperature in a transient thermal analysis

Creator
Creator

Hello,

 

I'm doing a thermal transient analysis and I'd like to know if it is possible to directly export the max temperature of a given group (or mesh) in relation to the time of the transient study. I've looked in the menus and it seems it is possible for the whole model, but not for a specific mesh or group...

 

Thanks,

 

Merlin

3 REPLIES

Re: Export max group temperature in a transient thermal analysis

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Merlin,

 

The NX Thermal mapping capability will allow you to exclude parts of the thermal model from being mapped to the structural fem, using groups.

 

Phil


Philippe Tremblay
phillippe.tremblay.ext@siemens.com
www.mayahtt.com

Re: Export max group temperature in a transient thermal analysis

Creator
Creator

Hello,

 

My problem does not concern a mapping for a thermal-structural analysis, I just want to automatically monitor the max temperature of a given group in relation to time when I do my post-processing of a transient thermal analysis.

 

Do you know how I can easily do that ?

 

Thanks

Re: Export max group temperature in a transient thermal analysis

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Merlin,

 

In the sim, under simulation object type, create a report. You can either track during solve, or by region after the solve is complete. You can select a gorup for each object.

 

The report will show you the max, min and average group temps for each time step.

 

Phil

 

27-Jul-15 3-30-58 PM.png


Philippe Tremblay
phillippe.tremblay.ext@siemens.com
www.mayahtt.com