Cancel
Showing results for 
Search instead for 
Did you mean: 

Export multiple subcases

Experimenter
Experimenter

I run nastran static simulation with a large number of subcases (>>10). I would like to export in a text file the same data (displacement results on a specific group) over all subcases in one operation. It was possible in IDEAS, is it with NX ?

2 REPLIES

Re: Export multiple subcases

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: Export multiple subcases

Experimenter
Experimenter

Thank you for the answer. I tried the Multiple Reduction command:

  • with the type graph, it wasn't possible to select nodes (to export displacements !)
  • with the type export, I have been able to create a universal file, but it's on the complete model

Maybe I am not using correctly the graph type!

 

Best regards