Cancel
Showing results for 
Search instead for 
Did you mean: 

Extracting the ATV matrix form INA analysis

Creator
Creator
As I want to analyze the Condition number and Rank of the ATV matrix. Therefore, it is required the ATV matrix in tabular form. So please suggest the procedure to get ATV matrix from the ATV solution set from Inverse numerical analysis
2 REPLIES

Re: Extracting the ATV matrix form INA analysis

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

You need to submit the job in manual mode.  Update the ATV solution, you will get a *.cmd file.   edit the file by adding a line "Export ATV Format Free File Sample.fre Return" to request exporting ATV results to a file sample.fre, which is in sysnoise free format.  See the following example. 

 

ENVIRONMENT SECTION SETUP USRDIR 'C:\Temp\' RETURN
ENVIRONMENT SECTION SETUP TMPDIR 'C:\Temp\' RETURN
Open Model 1 File ms2bub-431-Acoustic.sdb Original Return
Extract Summary Return
Environment Section SETUP GEO_TOLERANCE '0.5' Return
 Compute ATV
Frequency 100 To 200 LinStep 10
  Near 2
  Far 5
  Quadrature 2  2  1
 Return
Export ATV Format Free File Sample.fre Return
Close Return
New Model 1 File ms2bub-431-SignalFile.sdb Return
Save Return
Exit

Re: Extracting the ATV matrix form INA analysis

Creator
Creator
Thanks for your reply
I have followed the same steps as you mentioned but where I will get the ATV matrix which can I use for further analysis.
Thanks in advance