Cancel
Showing results for 
Search instead for 
Did you mean: 

FEM for multiple arrangements in part file

Experimenter
Experimenter

Does anyone know if there is a way to make a FEM for 2 different arrangements in a part assembly?

 

I can manually move the parts from the default arrangement that I made in the part file and the i_part and FEM will update accordingly. But, if I use the arrangements to move the parts, the i_part and the FEM will not update to these changes. Is there a way to make the i_part and the FEM to sync to multiple arrangements rather than having to manually move all the parts?

 

Thank you,

Laura

2 REPLIES
Highlighted

Re: FEM for multiple arrangements in part file

Legend
Legend

Are you using Assembly FEM?

Re: FEM for multiple arrangements in part file

Experimenter
Experimenter

TENTECHLLC,

 

No, I had used the make new FEM and simulation option.

 

Laura