Cancel
Showing results for 
Search instead for 
Did you mean: 

Flow paraller run MPICH2 error

Pioneer
Pioneer

Hello

 

im running a solution in paraller but getting this type of error:

 

unable to read the cmd header on the pmi context, Error = -1
.
Error posting readv, Etäpalvelin sulki aiemmin luodun yhteyden.(10054)
unable to read the cmd header on the pmi context, Error = -1
.
Error posting readv, Etäpalvelin sulki aiemmin luodun yhteyden.(10054)
unable to read the cmd header on the pmi context, Error = -1
.
Error posting readv, Etäpalvelin sulki aiemmin luodun yhteyden.(10054)
received suspend command for a pmi context that doesn't exist: unmatched id = 12
received suspend command for a pmi context that doesn't exist: unmatched id = 6
unable to read the cmd header on the pmi context, Error = -1

 

ob aborted:

rank: node: exit code[: error message]

0: Vortex: 123

1: Vortex: 123

2: Vortex: 123

3: Vortex: 123

4: Vortex: -1073741819: process 4 exited without calling finalize

5: Vortex: 123

6: Vortex: -1073740940

7: Vortex: 123

8: Vortex: 123

9: Vortex: 123

10: Vortex: 123

11: Vortex: 123

12: Vortex: 123

13: Vortex: 123

14: Vortex: 123

15: Vortex: 123

16: Vortex: 123

17: Vortex: 123

18: Vortex: 123

19: Vortex: 123

20: Vortex: 123

21: Vortex: 123

22: Vortex: 123

23: Vortex: 123

24: Vortex: 123

25: Vortex: 123

26: Vortex: 123

27: Vortex: 123

 

 

 

 

Same solution works on different computer. 

Any idea what could cause this problem?

 

 

 

11 REPLIES

Re: Flow paraller run MPICH2 error

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Check if you start the MPICH2 as Admin.

Re: Flow paraller run MPICH2 error

Pioneer
Pioneer

Hello

 

Did not do any difference.

I am already running with full admin/ full access.

 

Re: Flow paraller run MPICH2 error

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

A couple of questions:

 

  • Which OS are you running on?
  • What are the hardware specs?

 

Re: Flow paraller run MPICH2 error

Pioneer
Pioneer
Hello

Win7 professional 64bit.
14 core i7 00 intel. 64G ddr4.
Not over clocked



My first concern was processor, openmpi runs with out problems in linux wit
same machine.

Re: Flow paraller run MPICH2 error

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

It is possible that the MPICH2 is not correctly setup in Windows. Is the smpd service running in the task manager?

 

The installation instructions are available here: https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help#uid:xid1128419:index_advanced:id1245911:i...

 

Re: Flow paraller run MPICH2 error

Pioneer
Pioneer

Hello

 

Was not MPI problem at all.

 

Actually a way too big time step in simulation, it did not give any error from solver it self.

Just an MPI error, and it only does this on my workstation.

 

 

For some reason my NX setup on this workstation does not automaticly reduce timestep.

And after first initial step it crashes.

 

Is there a check box for automatic time step reduction that I have accedently disabled???

 

 

Re: Flow paraller run MPICH2 error

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Are you using the same solver patch on your machine as on the other machines? You can see the patch version at the top of the log file.

 

If the patches are the same, I would check whether you have sufficient memory to run the solve. Please try running with fewer cores and monitor the memory usage in the Task Manager.

Re: Flow paraller run MPICH2 error

Pioneer
Pioneer

Hello

 

Finite Element Model

--------------------

 

Solver type: Simcenter Thermal/Flow

Analysis type: Coupled Thermal-Flow

Solution type: Advanced Thermal-Flow

Simulation File: 

Solution: Solution_1

 

Number of nodes in thermal model: 0

Number of elements in thermal model: 0

 

Number of nodes in flow model: 129037

Number of elements in flow model: 594813

 

Number of fluid nodes reused for surface coating: 598

Number of elements created for surface coating: 1039

 

Solution Options

----------------

 

Steady-State Analysis

Solution Method: Concurrent

Communication Frequency: 1

Solving Flow

Solving Thermal

 

Ambient Temperature: 2.000E+01 C

Ambient Pressure: 1.014E+02 mN/mm^2

Gravitational Acceleration: 9.810E+03 mm/s^2

Gravity Direction: X: 0.000E+00 Y: 0.000E+00 Z:-1.000E+00

Fluid buoyancy: Off

 

Flow laminar/turbulent model: Mixing length

Length scale is auto calculated

 

Flow solver iteration limit: 1000

Flow converged when RMS residual less than: 2.000E-04

Flow solver physical time step: 1.000E-08 s

Flow solver heat imbalance: 2.000E-02

 

Advection Scheme Momentum: First Order

Advection Scheme Energy (if Solve_Energy): First Order

 

Global Relaxation Factor: 7.500E-02

Mass Relaxation Factor: 7.500E-03

Fluids Relaxation Factor: 9.000E-02

Turbulence Relaxation Factor: 1.000E-02

 

Freeze flow field: Off

High Speed Flow: On

Connect Disjoint Fluid Meshes: On

 

running on 28 procesess.

And Im only running 1/3 of my RAM capasity.

Re: Flow paraller run MPICH2 error

Pioneer
Pioneer

Yes Im runnig same solvers and everything.

It is actually same solution, at least copy of it.