Cancel
Showing results for 
Search instead for 
Did you mean: 

Font degradation after upgrading to Windows 10

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello NX Experts!,

After upgrading the laptop to Windows 10 I see a degradation in the quality of legend text during postprocessing results in NX AdvSim V10, how to improve the font quality?, thanks!.

 

font-degradation.png

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/
14 REPLIES

Re: Font degradation after upgrading to Windows 10

Siemens Phenom Siemens Phenom
Siemens Phenom

The font in the PostView can be adjusted using the controls (Automatic Font Scaling/Scale Factor) on the Post View Legend Text tab.

 

 

PostView.png

Re: Font degradation after upgrading to Windows 10

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Jim,

Not progress here, is not a problem related with font size, but font quality.

I do not see the way to change the font type used for postprocessing in order to see if using another font it will improve the font quality, I am searching under CUSTOMER DEFAULTS, but the option is not available, any suggestion? - thanks!.

 

CUSTOMER_DEFAULTS-postprocessing.png

 

Best regards,

Blas.

 

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Font degradation after upgrading to Windows 10

Phenom
Phenom

Dear Blas,

 

the problem you described also occurs in my software environment but in another configuration.

I use Windows7-64bit with NX 8.5.2 and the post processing fonts are well suited.

 

Now after installing NX 10 at the same Windows the font of text in post processing header lines degrade to something with missing pixels as you pictured. It looks like "using the wrong antialiasing - technique" when plotting the letters.

 

I am also very interested in a solution of this problem.

 

Greetings, Michael

Re: Font degradation after upgrading to Windows 10

Siemens Phenom Siemens Phenom
Siemens Phenom

The actual font used for the Post View legend text can be modified on the View, Visualization, Preferences dialog under Session Settings:

 

VisualizationPreferences-Session.png

Re: Font degradation after upgrading to Windows 10

Phenom
Phenom

Hi JimB,

thank your for answering.

The location of font setting and changing it is very interesting an sometime usefull, but it does not solve my problem.

After changing my visualization font the effect of degradation only changes its appearance in the other font style.

 

Appearance in NX8.5.2 with Arial:

NX8.5.2_Arial_001.png

Appearance in NX10 witrh Arial:

NX10_Arial_001.png

Appearance in NX10 with Times:

NX10_Times_001.png

Appearance in NX8.5.2 with Times:
NX8.5.2_Times_001.png

 

You see, same problem only in another style.

 

Could there be other reasons? - Any Suggestions? - May be graphical adapter?

 

Greetings, Michael

Re: Font degradation after upgrading to Windows 10

Siemens Phenom Siemens Phenom
Siemens Phenom

You can try turning off Automatic Scaling on the PostView Legend Text tab. If you can't obtain satisfactory results, please report the probelm via GTAC so that it can be tracked.

Re: Font degradation after upgrading to Windows 10

Phenom
Phenom

Hello JimB,

 

thank you for the suggestion but it does not work. I will report it to GTAC as you recommended, except Blas has already a solution or a solution request at GTAC.

 

@Blas: Did you already ask for help at GTAC?

 

I hope, they can cope it.

 

Best wishes, Michael

 

 

 

Re: Font degradation after upgrading to Windows 10

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

Not progress, the same problem here, not reported yet to GTAC.

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Font degradation after upgrading to Windows 10

Pioneer
Pioneer

Hello,

 

I had a similar problem. I don't remember what update it was after which the problem occurred but I found out, that in my case it was the "Line Antialiasing", just like Michael suspected.

 

Line_Antialiasing_on.PNG

"Line Antialiasing" turned on

 

 

Line_Antialiasing_off.PNG

"Line Antialiasing" turned off

 

 

Although the "Line Antialiasing" is then not availible for the lines, which should be the intended use, the font looks OK.

 

Hope that works for you and you can use it as workaround as long as the problem isn't fixed yet.

 

JockMcCool