Cancel
Showing results for 
Search instead for 
Did you mean: 

How to apply temperature pre-load using NX thermal results in NX10?

Experimenter
Experimenter

I'm using NX10. I have solved a thermal model, and mapped the temperatures to a structural model. I'm trying to solve the strucutral model using the mapped temperature result file (.bun) as a temperature load. However, in Solution - "Temperature Set" form, I couldn't specify any temperature distribution using the mapped temperature result file. In NX 9 or earlier version, I could do so though.  

2 REPLIES

Re: How to apply temperature pre-load using NX thermal results in NX10?

Siemens Phenom Siemens Phenom
Siemens Phenom

Nastran temperature loads were overhauled in NX 10 to consolidate everything into temperature load sets.

 

You need to create a Temperature Load set. In that set, you create a temperature load. You have several choices of Type:

 

Temperature (which can reference a spatial field for magnitude)

Node ID Table

A new External time unassigned, which can be a file reference to a solver results file

 

 

 

Re: How to apply temperature pre-load using NX thermal results in NX10?

Experimenter
Experimenter

Thanks for your quick reply. I'll use the temperature load option: "A new External time unassigned" for my problem. Does this mean if you have multiple temperature results, you have to manually create multiple temperature load sets and then solve?