Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create a 4D field in Simcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Quick Overview

You may have to define a load or a boundary condition that not only varies as a function of spatial coordinates, but also with time, temperature, or frequency. This Tips & Trick shows how to use Simcenter to create a 4D field, which allows you to model a functional expression of the form:

 

f = f(x1,x2,x3,α)

 

where x1, x2, and x3 represent a set of cartesian, cylindrical, spherical, or parametric spatial coordinates, and α represents a non-spatial variable like time, temperature, or frequency.

 

If the 4D functional relationship can be expressed as a closed-form mathematical expression, you can create the 4D field as a formula field. When Simcenter evaluates the formula field for a given set of spatial and non-spatial values, it simply evaluates the expression that relates the independent and dependent domains at the given values.

 

If the 4D functional relationship can be approximated by a set of tabular data that relates the independent and dependent domains, you can create the 4D field as a table field. When Simcenter evaluates the table field for a given set of spatial and non-spatial values at which a tabular data point does not exist, it interpolates the tabular data to obtain the corresponding dependent domain value. You can select the interpolation method that the software uses to look up values.

 

In this example we will show how to use a 4D formula field in Simcenter to model the footprint pressure of a roller traveling on a track.

Figure 1: Model the foot print pressure of a roller travelling on a track.

 

Figure 2: Varying pressure with spatial coordinates and time.

Steps

Let’s assume that the roller travels at a speed of 3 mm/sec and has a foot print pressure of 9 mm length (in the X axis) with a maximum pressure of 45 MPa.

 

1. Create a field of varying spatial coordinates with time  

 

Since the roller is moving at a constant speed of 3 mm/sec, the roller’s central location can be simply calculated using the following function:

 

X = 3*t

 

To create this field, in the Simulation Navigator right click on the Fields node and select New Field, Formula.

 

Figure 3: Create a formula field.

 

In the Formula Field dialog, under the Name group, enter a meaningful name, for example, X_Center. Then under the Domain group, set the Independent to time and Dependent to Cartesian.

 

Since in our model the position of the roller changes only along the X axis,  under the Expression group, select x and in the Rule Formula box type:

 

3[mm/sec]*time

 

Figure 4: Create a formula field for position of the roller with respect to time.

 

By end of this step, we defined the varying position of the roller with respect to time. So, we can now proceed to define the pressure field.

 

2. Create a field for the pressure

 

We assume that the roller footprint pressure is maximum at its center and linearly decreases toward the fore and aft edges of the foot print, in the X direction. The pressure is constant in the other direction on the surface.

 

Figure 5: Roller footprint pressure distribution.

 

To define a field for the pressure, in the Simulation Navigator right click on the Fields node and select New Field, Formula.

 

In the Formula Field dialog, under the Domain group, set the Independent to time,Cartesian and Dependent to Pressure. You will notice that the independent variables and the field created in the step1 are listed under the Expression group.

 

We assumed the roller foot print pressure has a length of 9 mm. So, the the pressure formula can be defined as  

 

if ( abs(x-fd(“X_center”,“x”))<=4.5) Then (10*(4.5-abs(x-fd(“X_center”,“x”)))) Else (0)

 

where x is the independent variable, and X_center is the position of the roller, which is varying with time according to the field defined in step 1. Note that to use a value from another field, you need to use the fd(“Fieldname”,”value”) command.

 

Figure 6: Define a formula field for the roller foot print pressure.

 

3. Define the pressure load

 

To define the pressure load, in the Simulation Navigator, right click on Loads, and select Pressure.

 

Figure 7: Define the pressure load.

 

Figure 8: Pressure dialog.

 

In the Pressure dialog, under the Model Objects group, select the track bed face as the location where the pressure should be applied. Under the Magnitude group, click on the equal sign, and then choose Select Existing Field.

 

Figure 9: Fields dialog.

 

In the Fields dialog, select the Formula Field, which was defined in Step 2. Click OK on all dialogs.

 

4. Verify the defined pressure (Optional)

 

By the end of step 3, the varying pressure with respect to spatial coordinates and time is already defined and can be used in a solution. Simcenter allows you to plot and animate the applied load to verify whether it is correctly defined and applied to the model.

 

To plot the varying pressure load, in the Simulation Navigator, right click on the pressure load and select Plot Contours.

 

Figure 10: Plot load contours of the applied pressure.

 

Figure 11: Boundary Condition Contour Plot dialog.

 

In the Boundary Condition Contour Plot dialog, under the Selected Boundary Conditions group select the pressure load. Then under the Plot Options group set the Plot Type to Animation, and Independent Variable to Time. Set the Start, Stop, and Number of Frames to 0, 100, and 33, respectively. Click on the Plot icon.

 

 

Figure 12: Contour plot of the applied pressure.

Maya Simulation: T +1.514.369.5706 | info@mayahtt.com | http://www.mayasimulation.com
4 REPLIES

Re: How to create a 4D field in Simcenter

Experimenter
Experimenter

Thank you for this clarification.

 

It seems that most of the solution types does in Simcenter (109 Direct transient, 129 Non-linear transient or 601,129 Non-linear transient) does not support boundary condition defined using 4D field. What is your recommendation of solving a case with such a 4D field?

 

NX 10.0.3.5 is in use.

Re: How to create a 4D field in Simcenter

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello,

 

SOL 601,129 supports tables of fields for pressure loads: As a minimum, you can create different spatial fields and add  time as an independent variable, as a new field.

 

4D field support is broadened in NX11, more will be supported in NX12. There are bondary confiditions that simply cannot be created in 10 that will be possible in future releases.

 

If there is a specific load you wish to create and a solution in mind, please let me know.

 

Phil


Philippe Tremblay
phillippe.tremblay.ext@siemens.com
www.mayahtt.com

Re: How to create a 4D field in Simcenter

Experimenter
Experimenter

Hi Phil

Thank you for your reply. Your minimum suggestion most probably works very well for now. It sounds rational that more features related to this are developed in the following versions.

 

In this case, I am running an analysis with a constant force on a beam which spatially moves from one end of a beam to another. Static solution in each step is adequate. I did it coarsely with sol 101 pointing a force to a multiple locations. Only I was considering if it could be done more neatly by applying a time-dependent function on this force movement. Then density of steps would be easy to control via expressions.

 

Mikko

 

 

Re: How to create a 4D field in Simcenter

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Perhaps the load definition would be more convenient that way, however solving dynamic, nonlinear or dynamic-nonlinear problems is far more demanding than simple linear solutions, from both computational and FE knowledge points of view. 


Philippe Tremblay
phillippe.tremblay.ext@siemens.com
www.mayahtt.com