Cancel
Showing results for 
Search instead for 
Did you mean: 

How to solve a pure moment example

Experimenter
Experimenter

I am try to solve an example with 2 moment at the end of the body , but it give error 

how can i mesh this problem  i think the error in the mesh 

 

i use 3d mech bec the part has a thickness 10 mm 

 

3 REPLIES

Re: How to solve a pure moment example

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

 

Try to apply the moment on one point/node. Use RBE2 or RBE3 to connect this node to the desired surface.

and check if your boundary conditions at the other end is valid (all fixed for example)

 

Best,

Sami

Re: How to solve a pure moment example

Experimenter
Experimenter
thankks sami
but how can we use RBE2 OR RBE3

Re: How to solve a pure moment example

Siemens Phenom Siemens Phenom
Siemens Phenom

3D solid element formulations only define translational stiffness at connected nodes, so you cannot apply a moment load to a node that is connected to only solid elements.

 

The suggestion is to create a point (or node) at the location where the neutral axis intersects the face that you want to apply a moment load on. Create a Point to Face (or a node to node) 1D connection from this point (or node) to the face (or all of the nodes on the face). Specify that the connection element type be RBE2 or RBE3.

 

Note that the instructions within parenthesis above are for an FE only model with no underlying geometry available.