Cancel
Showing results for 
Search instead for 
Did you mean: 

How we can export material from local materials created in NX FEM to specified Dirrectory??

Experimenter
Experimenter

Hello Experts,

 

I have created a material in NX FEM and want to export same material outside NX in specified directory as MAT Card in *.xml format. How we can do it??

 

Best Regards,

Raje

6 REPLIES

Re: How we can export material from local materials created in NX FEM to specified Dirrectory??

Siemens Phenom Siemens Phenom
Siemens Phenom

Raje,

 

Use Manage Library Materials. Set Type to Export Material to Library, specify a .xml filename, set the Source Material List to Local Materials and select the material(s) that you want to export.

 

MaterialExport.png

 

Regards,

Jim

 

Re: How we can export material from local materials created in NX FEM to specified Dirrectory??

Experimenter
Experimenter

Jim,

 

Thanks for the solution.

 

I am trying the same procedure in NX8.5. I have specified Stress/Strain data in material card, but once I export that card and import in another session of NX8.5 then its not able to show defined stress/strain data.

 

Though I tried the same with NX8 and its working fine but not in NX8.5.

 

Regards,

Raje

 

Re: How we can export material from local materials created in NX FEM to specified Dirrectory??

Siemens Phenom Siemens Phenom
Siemens Phenom

Raje,

 

This sounds like it may be a bug. Does the .xml file contain the stress-strain data? If not, then it is an export error. If so, then it is an import error. Either way, please contact GTAC so that they can investigate and submit a PR if necessary.

 

Regards,

Jim

 

Re: How we can export material from local materials created in NX FEM to specified Dirrectory??

Experimenter
Experimenter

Hi

 

I have same problem with export /import of stress-strain data in my .xml file (NX8.5).

Is there any solution for this bug?

I didn't find any stress strain data in .xml file.

 

Regards,

Matej

Re: How we can export material from local materials created in NX FEM to specified Dirrectory??

Creator
Creator

There is a solution. Use the NX10 release to create a new material (in the local materials) with the desired stress-strain diagram. Then export this material to the specified NX Material Library (xml-file). You can use this library also with the NX8.5 release and the stress-strain diagram will be feasible!

Re: How we can export material from local materials created in NX FEM to specified Dirrectory??

Experimenter
Experimenter

Hi.

PB, thanks for advice, but unfortunately my company will switch to NX 10 next year.

I solved this problem in this way that I have Stress-Strain curve saves as F[x] Fields. So

I don’t have to type in all points manually every time.

 

Regards, Matej