Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Import csv like results in NX

Phenom
Phenom

Hello,

 

I am not a NX user but I have a problem related to NX:

I have a custom post-processing tool which generates nodal scalar output for FEMAP in CSV format, which is basically:

 

dataset delimiter

header (titles)

node ID   vec1   vec2 ... vecK

  |                |          |            |

  |                |          |            |

           ...etc...

dataset delimiter

 

Is there a way to import this easily in NX? perhaps not coma-separated, maybe space separated?

If possible my goal is to avoid the UNV format, and stick with a format close to the one above.

I do not have acces to NX's help, sorry if the answer is obvious.

 

Any ideas?

 

Thanks for your help,

 

Adrien

4 REPLIES

Re: Import csv like results in NX

Siemens Phenom Siemens Phenom
Siemens Phenom

Adrien,

 

To help determine how to proceed, can you tell us what you need to do with the results inside of NX. For example, do you need to generate a contour plot or an X-Y plot, or will you use the results as a boundary condition on a subsequent analysis, etc.

 

Regards,

Jim

 

Re: Import csv like results in NX

Phenom
Phenom

Hi Jim,

 

Thanks for the quick response!

I would like to generate contour plots of the scalar data.

 

I have no notion whatsoever of how NX organises output. The FEMAP CSV is organised with outputsets and outputvectors: the outputset is a collection of vectors, the vector is the actual output data

 

Adrien

Re: Import csv like results in NX

Siemens Phenom Siemens Phenom
Siemens Phenom

Adrien,

 

The only way to directly generate a contour plot from results is to use a .unv file. Since you've said that you want to avoid this, here are a couple of other options:

 

1) You can import CSV data into a Table Field. The display of a table field allows you to visualize the distribution and relative magnitude of the data:

 

Table Field Dialog

 

FieldDisplay.png

 

However, there is no color bar and you cannot probe the values in this display. You can map a table field onto a boundary condition, such as nodal temperatures or element pressures. You can then contour plot the magnitude of that boundary condition as a standard Post Processing display that can be queried:

 

 

NodalTemperatureDialog.png

 

NodalTemperaturePlot.png

 

ElementPressureDialog.png

 

ElementPressurePlot.png

 

Regards,

Jim

 

Re: Import csv like results in NX

Phenom
Phenom

Hmm OK, I'll compromise and accept the UNV.

 

I'm only familiar with the dataset 2414 which was the custom tensorial output back when I used it.

It could have nodal and elemental output, but always written in 6 columns.

 

I would like to make it as similar as possible to the FEMAP CSV, espacially so I don't have to modify my programme's underlying architecture.

 

Here's what I have in mind, will this work? (I'm using the unv specification from Cincinnati SDRL, not sure if it's still applicable...)

 

Datasetclass = data at nodes

I have 64 output vectors, so for each node, 64 values

 

1) Can I write this in only 1 dataset  2414? (from the spec I assume yes - very important point!!)

2) Do I have to write it in 6 columns? (from the spec I assume yes)

3) How are titles handled? (as to that I have no clue)

 

Thank you very much for your help