Cancel
Showing results for 
Search instead for 
Did you mean: 

Linear vs Non Linear Stress for Fatigue

Experimenter
Experimenter

New to fatigue analysis and have a few fundamental questions of anyone would care to comment. Based on what I think I know is that a (S-N) stress based approach is best for high cycle fatigue and a (E-N) strain based approach for low cycle fatigue. The cut off generally being around 100K cycles.

 

Stress Based Approach

For high cycle fatigue I am using a (S-N) approach because the linear stresses are below 70% of yield and in the elastic part of the material curve. I clearly understand this no problem.

 

Strain Based Approach

When the linear stresses are over yield this is where I am still unclear and have questions.

 

  1. Should I always use a strain based approach when the stress is over yield?
  2. Should I use the above linear stresses, over yield, with an elastic plastic correction?
  3. Should I use non-linear stress results with no elastic plastic correction.

 

Any comments would be appreciated.

8 REPLIES

Re: Linear vs Non Linear Stress for Fatigue

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

cadguy,

 

You should be using strain life when the maximum stress exceeds the yield strength of your material.

 

You can use either linear and nonlinear results, and in both cases the software will apply an elastic-plastic correction. You need to check on 'Use Non-Linear Results' in the Solve Options tabs for the nonlinear results to be considered.

 

If you elect to use nonlinear results, you should not be defining a notch factor.

 

Phil


Philippe Tremblay
phillippe.tremblay.ext@siemens.com
www.mayahtt.com

Re: Linear vs Non Linear Stress for Fatigue

Experimenter
Experimenter

Thanks for the feedback.  When I use the non linear stress option should i use the transient durbaility option?  If so how does the force get fully reversed?

 

I could run the load non linear and reverse the load to get a full cycle, however, I have 5 load points so it is very complex?

 

Would you just take the peak stress from the non linear and full reverse it kind of like a linear analysis?

 

Thanks

Re: Linear vs Non Linear Stress for Fatigue

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You can extract stresses/strains from either a static or a transient solution. You would define a transient or static durability event accordingly.

 

In a transient event, the reversals are determined by the response history and by the subsequent rainflow counting.

 

In a static event, you define the reversals by selecting a pattern type, full or half cycle. The stresses (linear or nonlinear) follow the same pattern.


Philippe Tremblay
phillippe.tremblay.ext@siemens.com
www.mayahtt.com

Re: Linear vs Non Linear Stress for Fatigue

Siemens Genius Siemens Genius
Siemens Genius

Dear cadguy, hi Phillippe,

 

let me add a little on the background of strain-life approaches.

 

First, everything about the limitation of the range of usage of stress-life approach is correct.

 

People found some 50-70 years ago that indeed the damage correlates better with the local strain history than with the local stress history, so above yieling one should have a look at strain-life approaches.

 

But for application, people also see that the yielding is typically only local (as one has does not design parts that see permanent plastic deformation in the range of fatigue loads). Therefore the strain-life methods also include approximation formulae (typically Neuber or ESED) that locally give a good approximation for the plastic behavior. In most cases this means elasic FE is enough. From our experience transient results are needed whenever

  • geometric non-linearities (e.g. contact)
  • high pre-loads (e.g. bolting)
  • large deformations

play a role. I.e. effects that can not be handled by locallized approximation.

 

Hope this helps

 

Michael

 

Let me also invite you to our parallel forum

http://community.plm.automation.siemens.com/t5/LMS-3D-Simulation-Solutions/bd-p/LMS-3D-Simulation

 

Dr. Michael Hack

Product Line Manager Durability Solutions

Simulation & Testing Solution

Siemens PLM Software

Dr.Michael Hack
Business Product Line Manager Durability
Simulation and Testing Solutions

Re: Linear vs Non Linear Stress for Fatigue

Builder
Builder

Hi Phil,

 

So does that mean the software apply plastic correction factor automatically without the need to be checked by the user?

 

For nonlinear analysis, do you mean that we check NLstress results as shown the attached? If so, what is the difference from performing this option (static sol101+ check the NLstress results in the Bulk entry) and the Nonlinear analysis S106, which also could be used combined with durability instead of the notch factor input? 

 

Mark, I do not know why I do not have access to the link you provided in the post above.

 

Thanks and Regards

Re: Linear vs Non Linear Stress for Fatigue

Pioneer
Pioneer
Hi,
the adress above leads to a non available location: https://community.plm.automation.siemens.com/t5/Forum-3D-OLD/bd-p/LMS-3D-Simulation, with the following statement "You do not have sufficient privileges for this resource or its parent to perform this action. Click your browser's Back button to continue. "

Would there be another location for your forum?
best regards
Cyril

Re: Linear vs Non Linear Stress for Fatigue

Siemens Genius Siemens Genius
Siemens Genius

Dear Cyril,

 

we have merged the forums in the meantime, so the LMS one does not exist anymore

 

Best Regards

 

Michael

Dr.Michael Hack
Business Product Line Manager Durability
Simulation and Testing Solutions

Re: Linear vs Non Linear Stress for Fatigue

Pioneer
Pioneer
OK, noted! Thank you and have a nice evening!
Cyril