cancel
Showing results for 
Search instead for 
Did you mean: 

Mapping Temperature data From text file

Pioneer
Pioneer

hai everyone 

 

I Am having a text file with temperature data along with the coordinate

ie 

X axis Y axis Z axis Temp

 

in the above format 

I want to use this data file in my simulation as load, how to map this data on to my FEM(both are of same geomentry) the text file is from other package

 

thank you

Karthik

1 REPLY

Re: Mapping Temperature data From text file

Siemens Phenom Siemens Phenom
Siemens Phenom

You can import the data directly into a table field with an independent domain of Cartesian and a dependent domain of Temperature.

 

If the coordinates in the file correspond to the node locations in the model, set the interpolation method to Nearest Neighbor.

 

Reference this table field in the temperature load.

 

The easiest way to create the field is in context. Create a temperatre load, set the distribution to Field and pick the option to create a new table field. There is a button on the table field dialog to import data from a file.