Cancel
Showing results for 
Search instead for 
Did you mean: 

Methodical model compare in the structure - replica

Experimenter
Experimenter
Hello Community! My name is Tobi and I work as a designer for automotive parts. Since 3 months I am using NX 10 at the beginning I had a Training afterwards I helped myself by searching in the Internet or reading articles/books. By now everything works fine I really like the program but from time to time there are some Points I dont find any solution... Task: - I have a Basic Modell. The structure and the order in the part Navigator is the Standard. - I also have modified Versions / revisions that shall contain this structure with absolutely the same Content / Details -> Features / measures. The order may differ at the Position where a modification was built in. - My aim is to check the modified part if it is absolutely identic constructed (except the additional areas) and if not to correct the differences (all fetures / measures etc.) - it would be perfect if I could also see if f.e. the number of selected faces for a Feature ist also the same !? my idea: - I know about the Option to Export a spreadsheet to Excel with the whole structure of the part Navigator - I also know about the possbility to Export all the expressions with measurements (in the form of "p1234") to a spreadsheet - I am looking for a way to get the whole Navigator table with all the appropriate Details in order of the structure so that I finally can compare the construction of my Basic part with my modified part - in the end I could adjust all differences Notes: - it is not enough just to check the model graphically I really Need to recreate the identic structure expect the modifications - the Basic part and the modified Versions are already existing and are changed continous - the extent of the parts is to big to check it manually by clicking through the structure - perhaps there is a better plan to reach my aim... Thank you in advance! Best regards from Germany. Tobi
3 REPLIES

Re: Methodical model compare in the structure - replica

Experimenter
Experimenter
Hello Community! My name is Tobi and I work as a designer for automotive parts. Since 3 months I am using NX 10 at the beginning I had a Training afterwards I helped myself by searching in the Internet or reading articles/books. By now everything works fine I really like the program but from time to time there are some Points I dont find any solution... Task: - I have a Basic Modell. The structure and the order in the part Navigator is the Standard. - I also have modified Versions / revisions that shall contain this structure with absolutely the same Content / Details -> Features / measures. The order may differ at the Position where a modification was built in. - My aim is to check the modified part if it is absolutely identic constructed (except the additional areas) and if not to correct the differences (all fetures / measures etc.) - it would be perfect if I could also see if f.e. the number of selected faces for a Feature ist also the same !? my idea: - I know about the Option to Export a spreadsheet to Excel with the whole structure of the part Navigator - I also know about the possbility to Export all the expressions with measurements (in the form of "p1234") to a spreadsheet - I am looking for a way to get the whole Navigator table with all the appropriate Details in order of the structure so that I finally can compare the construction of my Basic part with my modified part - in the end I could adjust all differences Notes: - it is not enough just to check the model graphically I really Need to recreate the identic structure expect the modifications - the Basic part and the modified Versions are already existing and are changed continous - the extent of the parts is to big to check it manually by clicking through the structure - perhaps there is a better plan to reach my aim... Thank you in advance! Best regards from Germany. Tobi

Re: Methodical model compare in the structure - replica

Experimenter
Experimenter
Hello Community! My name is Tobi and I work as a designer for automotive parts. Since 3 months I am using NX 10 at the beginning I had a Training afterwards I helped myself by searching in the Internet or reading articles/books. By now everything works fine I really like the program but from time to time there are some Points I dont find any solution... Task: - I have a Basic Modell. The structure and the order in the part Navigator is the Standard. - I also have modified Versions / revisions that shall contain this structure with absolutely the same Content / Details -> Features / measures. The order may differ at the Position where a modification was built in. - My aim is to check the modified part if it is absolutely identic constructed (except the additional areas) and if not to correct the differences (all fetures / measures etc.) - it would be perfect if I could also see if f.e. the number of selected faces for a Feature ist also the same !? my idea: - I know about the Option to Export a spreadsheet to Excel with the whole structure of the part Navigator - I also know about the possbility to Export all the expressions with measurements (in the form of "p1234") to a spreadsheet - I am looking for a way to get the whole Navigator table with all the appropriate Details in order of the structure so that I finally can compare the construction of my Basic part with my modified part - in the end I could adjust all differences Notes: - it is not enough just to check the model graphically I really Need to recreate the identic structure expect the modifications - the Basic part and the modified Versions are already existing and are changed continous - the extent of the parts is to big to check it manually by clicking through the structure - perhaps there is a better plan to reach my aim... Thank you in advance! Best regards from Germany. Tobi

Sorry for this lousy post...

Experimenter
Experimenter
Sorry guys! Have to train how to do Posts in this Forum... Plae for mercy. Tobi