Cancel
Showing results for 
Search instead for 
Did you mean: 

Modeling time varying force

Creator
Creator

Hello

 

I am trying to use NX to model a time varying force. Specifically, I am trying to model a structure subjected to a gust of wind at 100 mph for 3 seconds.

 

Can this be done with the advanced simulation tool, or does this type of modeling require the response simulation add-on module? If you can do this with the advanced simulation tool, how do you account for the time?

 

Thank you....

1 REPLY

Betreff: Modeling time varying force

Phenom
Phenom

Hi Michael,

 

first of all you have to use Solution 601 /129 or 701 to solve problems with time characteristics and large gradients of loads in short time.

Mostly you are able to specify a time characteritic in solution => case control

-  strategy parameters and

- time step definitions and additionally

in load description, (may be a pressure  with time domain table or field to describe time chraracteristics).

 

In my opinion you can do it in advanced simulation without response simulation. It depends on your problem.

 

Best wishes,

Michael

 

Production: NX10; Development: VB, TCL/TK, FORTRAN; Testing: NX11
Kudos for good posts! And if you find my post helpful, and it answers your question, please mark it as an "Accepted Solution"