Cancel
Showing results for 
Search instead for 
Did you mean: 

Motion Simulation - Cannot select relative link for trace

Experimenter
Experimenter

 Hi, when trying to create a trace of a marker with another link as the reference i get the error message, that the "obects selected are already defined", as i have already created an trace with an absolute reference frame. It seems to me the selection dialog of the Reference frame wont work, as it does not seem to allow the selection of another link.

 

The Marker references the link "Blechteil_Z", the reference frame for the trace is supposed to be "Presse", these two are not connected.

 

Also sometimes random objects get selected when switching from "absolute reference" to "select link" in the dialog...

 

i am using NX 9.0.1.3