Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 10 Block UI Styler: Property Expanded of a group

Creator
Creator

Hello everyone!

I have created a dialog using the Block UI Styler. The dialog contains a group with a couple of elements inside. I want this group to be minimized, when the dialog is started. Therefore, I set the property called Expanded to be False. But instead of becoming minimized the group simply disappears from the dialog. Is there a solution for this? Thank you very much!

Best Regards

6 REPLIES

Re: NX 10 Block UI Styler: Property Expanded of a group

Siemens Phenom Siemens Phenom
Siemens Phenom

The expanded property should do what you want. The show property should do what you are describing as happening. Are you sure you've set the right one?

Re: NX 10 Block UI Styler: Property Expanded of a group

Creator
Creator

Hey JimB,

 

the show property is set to be true. Just to make it clear i've taken the screenshots.

This is what I want to get, namely I want subgroup 2 to be minimized:

 

Wanted.png

 

This is what I get, setting the Expanded property of the subgroup 2 to False:

 

Result.png

 

Here are the properties:

 

Properties.PNG

 

 

Re: NX 10 Block UI Styler: Property Expanded of a group

Siemens Phenom Siemens Phenom
Siemens Phenom

Are their active blocks in Subgroup 2's container item list?

 

It may be best to post the .dlx file and the source code.

Re: NX 10 Block UI Styler: Property Expanded of a group

Creator
Creator

Yes, there are. The files are attached.

 

Re: NX 10 Block UI Styler: Property Expanded of a group

Siemens Phenom Siemens Phenom
Siemens Phenom

I think you are running with Groups (Less). Click on the settings icon in the upper left corner of the dialog. Check either 'Groups (More)' or 'Show Collapsed Groups'

 

groups.png

Re: NX 10 Block UI Styler: Property Expanded of a group

Creator
Creator
Yes, that was it! Thanks a lot!