cancel
Showing results for 
Search instead for 
Did you mean: 

NX Motion Simulation: Load Transfer - bearings problem

Experimenter
Experimenter

Hi,
may anyone know how to make shaft rest on two bearings simultanoeusly?
To obtain rotational motion NX needs only one base, however, I would like to receive forces in two bearings. After using "Menu/Analysis/Motion/Load Transfer" option I get forces only in one bearing cause the other one is treated as redundant.

I would like to model a shaft on two bearings, load it and than switch to Advanced Analysis and create structural analysis of the bearing using results from Motion. Unfortunately, I get all forces in only one bearing.

1 REPLY

Re: NX Motion Simulation: Load Transfer - bearings problem

Siemens Creator Siemens Creator
Siemens Creator

Right, there are redundant Degrees Of Freedom. Recommendation in your scope is to replace the Joints by cylindrical bushings with very high stiffness and damping in all directions except the torsional. For example:

Radial Stiffness to 1E7 N/mm with damping at 1E5 N.s/mm.

Torsional 1 N.mm/deg, damping 1000 N.mm.sec/deg

 

Gilles Dubourg
Product Manager – Simcenter 3D Motion
Product Lifecycle Management
Siemens Industry Software SAS
gilles.dubourg@siemens.com
www.siemens.com/plm