cancel
Showing results for 
Search instead for 
Did you mean: 

NX Nasrtan Thermal/Flow

Experimenter
Experimenter

Hi everybody! 

Anybody knows what does mean this note in attached file? Thk. 

 

Thermal/Flow Analysis
=====================
MAYA Heat Transfer Technologies Ltd.


TMG Thermal/Flow 10.0.112 Nov 05 2014


Run directory specified for analysis:
E:\Program Files\Siemens\NX 10.0\NXCAE_EXTRAS\tmg\exe\

NX2TMG - Thermal/flow model file builder
======================================================================
Time: Tue Apr 25 11:24:29 2017

+--------------------------------------------------------------------+
| Model Builder |
+--------------------------------------------------------------------+

Reading model file...
...model file read.

+--------------------------------------------------------------------+
| Model Summary |
+--------------------------------------------------------------------+

Finite Element Model
--------------------

Solver type: NX THERMAL / FLOW
Analysis type: Thermal
Solution type: Thermal
Simulation File: C:\Users\123\Desktop\Rabota\test\1\assyfem1_sim1.sim
Solution: Solution_1

Number of nodes in thermal model: 108
Number of elements in thermal model: 42

Number of nodes in flow model: 0
Number of elements in flow model: 0

Number of elements created for surface coating: 74

Solution Options
----------------

Steady-State Analysis

Solving Thermal

Ambient Temperature: 2.000E+01 C
Ambient Pressure: 1.014E+02 mN/mm^2
Gravitational Acceleration: 9.810E+03 mm/s^2
Gravity Direction: X: 0.000E+00 Y: 0.000E+00 Z:-1.000E+00

Performing mesh checks...

- interior and warping angle
checks on fluid elements...
...angle checks on fluid
elements completed.

- interior and warping angle
checks on thermal elements...
...angle checks on thermal
elements completed.

- coincident node check
on fluid model...
...node check on fluid
model completed.

- coincident node check
on thermal model...
...node check on thermal
model completed.

- coincident element check
on fluid model...

... coincident fluid elements
check completed.

...mesh checks completed.

Thermal Boundary Conditions
---------------------------

Number of thermal boundary conditions: 2

Thermal Boundary Condition Type Value FSF TCP
----------------------------------------------------------------------
1 - Thermal Load(1) Heat Load 1.000E+06 mN-mm/s No No
1 - INIT_BC Initial Temp 2.000E+01 C No Yes
1 - Radiation(1) Radiative 2.000E+01 C No No

Thermal Couplings
-----------------

Number of thermal couplings: 2

Thermal Coupling Name Value Units
----------------------------------------------------------------------
1 - Interface Resistance(1) 1.750E+09 mN/mm-s-C
Type: Interface, Heat Transfer Coefficient
Primary Area: 7.000E+03 mm^2
1 - Face Contact(1)
Type: Surface to Surface Contact, Perfect
Primary Area: 9.000E+02 mm^2
Secondary Area: 7.000E+03 mm^2
----------------------------------------------------------------------

Writing thermal model files...
...done.

Executing Thermal Solver Only

THERMAL - Thermal analysis
======================================================================
Time: Tue Apr 25 11:24:30 2017


+--------------------------------------------------------------------+
| Solving Thermal Model - Elapsed Time: 00 min 01 sec |
+--------------------------------------------------------------------+

** FATAL ** Error file tmgmsg.dat not found, $SDRC_TMG possibly incorrectly defined
** FATAL ** Error writing message 1206 to MSGF
** FATAL ** Error file tmgmsg.dat not found, $SDRC_TMG possibly incorrectly defined
** FATAL ** Error writing message 2722 to MSGF
** FATAL ** Error writing message 2722 to MSGF
** FATAL ** Error file tmgmsg.dat not found, $SDRC_TMG possibly incorrectly defined
** FATAL ** Error writing message 1015 to MSGF


Run aborted due to fatal errors.


+--------------------------------------------------------------------+
| END |
+--------------------------------------------------------------------+

Solution elapsed time: 00 min 06 sec

1 REPLY

Re: NX Nasrtan Thermal/Flow

Community Manager Community Manager
Community Manager
Hi,

Well for one, this isn't NX Nastran but NX Thermal (TMG) that you are using. It would appear that you don't have it setup correctly. Do you have access to the NX Thermal licenses?

Regards,
Ganesh

Simcenter 3D Community Manager
Simulation and Test Solutions