Cancel
Showing results for 
Search instead for 
Did you mean: 

[NX11] How to hide the element edges of the mesh in a result plot?

Experimenter
Experimenter

Hi,

 

Due to the mesh density, the elements edges hide the results in a results plot.

I like to either hide element edges/mesh, or plot results on the geometry bodies or any other option that actually lets mee see the results without having to zoom in until I only have a small part of the model in sight.

 

Can anyone help me with this issue please?

 

Regards,

Rogier

9 REPLIES

Re: [NX11] How to hide the element edges of the mesh in a result plot?

Siemens Phenom Siemens Phenom
Siemens Phenom

Rogier,

 

Edit the Post View from the Post Processing Navigator or select Edit Post View from the Results ribbon. Then go to the Edges and Faces tab. Set the edges option to Feature or None to limit the display of element edges in the post view.

 

Regards,

Mark

 

 

Mark Lamping

Simulation Product Management

Simulation and Test Solutions

 

Siemens Industry Sector

Siemens Product Lifecycle Management Software Inc.

 

mark.lamping@siemens.com

www.siemens.com/plm

Re: [NX11] How to hide the element edges of the mesh in a result plot?

Experimenter
Experimenter

Thank you!

 

So simple. How did I miss that...

Re: [NX11] How to hide the element edges of the mesh in a result plot?

Pioneer
Pioneer

"Edit the Post View from the Post Processing Navigator or select Edit Post View from the Results ribbon"

 

I could not locate this option on Femap v11.2. Is there a short cut key to access the Edges and Faces tab?

 

Thanks, Su

Re: [NX11] How to hide the element edges of the mesh in a result plot?

Siemens Phenom Siemens Phenom
Siemens Phenom
This is the Simcenter forum and the instructions were for doing this and Simcenter.

If you would like to know how to do this in Femap, please post the question in the Femap forum.

Re: [NX11] How to hide the element edges of the mesh in a result plot?

Pioneer
Pioneer

Thanks for that information!

 

Best regards,

Su

Re: [NX11] How to hide the element edges of the mesh in a result plot?

Genius
Genius

I switch between Element edges and Feature edges a lot so I created a couple of partial post processing templates so that I don't have to use the edit menu. The templates I created are in the attached zip file.

Re: [NX11] How to hide the element edges of the mesh in a result plot?

Pioneer
Pioneer

Thanks for sharing those templates. But I have no idea how to include and use them in Femap. Could you please share some information about this?

Re: [NX11] How to hide the element edges of the mesh in a result plot?

Siemens Phenom Siemens Phenom
Siemens Phenom

This is the NX Simulation forum. You will have to post your question in the Femap forum for help with that product.

 

Re: [NX11] How to hide the element edges of the mesh in a result plot?

Pioneer
Pioneer

Sorry Jim.