Cancel
Showing results for 
Search instead for 
Did you mean: 

No NX10 tutorial for SOL111?

Phenom
Phenom

To all,

 

Does any one know if there is a tutorial (step-by-step example) to set up a SOL111 with NX10? I cannot find anything. It looks like the day of a templates calling an INCLUDE files are gone and everything has to be done from GUIs. Overcomplicate evertything!

 

I had a good look around the examples/exercises/lessons but cannot find anything.

 

Thanks

Regards

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)
3 REPLIES

Re: No NX10 tutorial for SOL111?

Siemens Phenom Siemens Phenom
Siemens Phenom

Not quite a tutorial, but hopefully it helps:

 

NX Nastran dynamics workflow

 

Specifying forcing frequencies for a frequency response analysis

 

Note that you can also use User Defined Text objects to reference external INCLUDE files into the solution:

 

Customizing a Nastran input file with user defined text

Re: No NX10 tutorial for SOL111?

Phenom
Phenom

Thanks JimB. I managed to set up (almost) everyting before I aksed the question. I am/was after the steps to create the dynamic excitation. Does not appear to be logical in NX. (My logic is flawed most likely or I am stuck in the Patran days!)

Production: NX9.0.3.4, NX10.0.2.6
Development: VB.NET (amateur level !)

Re: No NX10 tutorial for SOL111?

Legend
Legend

We typically have random and SRS done by hand, i.e. created in a text editor.  Doing this in NX is too tedious in my opinion, not NX's fault, but rather the convoluted NASTRAN card interaction...