Cancel
Showing results for 
Search instead for 
Did you mean: 

Node ID

Experimenter
Experimenter

Dear,

 

Below you may find a summary of a mesh. Note that the total number of nodes is smaller than the max node label. Further the node labeling does not start at 1. 

 

Is it possible to force NX to renumber the nodes prior to writing the input deck? Such that the max node label is the same as the number of nodes and the min node label is 1.

 

Regards,

Karim

 

 

 

MESH SUMMARY
------------

Total number of elements in the part : 166408
Total number of nodes in the part : 322975
Number of Rigid Link elements : 2
Number of Tetra10 elements : 166406
Minimum element label used : 146379
Maximum element label used : 312786
Minimum node label used : 59445
Maximum node label used : 600892

1 REPLY

Re: Node ID

Experimenter
Experimenter

So posted a bit to fast. After overlooking it several times I just found the solution:

 

The function "Reset Node and Element IDs"

 

This gave the following solution:

 

MESH SUMMARY
------------

Total number of elements in the part : 166408
Total number of nodes in the part : 322975
Number of Rigid Link elements : 2
Number of Tetra10 elements : 166406
Minimum element label used : 1
Maximum element label used : 166408
Minimum node label used : 1
Maximum node label used : 322975

 

 

Regards, Karim