Cancel
Showing results for 
Search instead for 
Did you mean: 

Orbital temperature range in space thermal system

Creator
Creator

Hi, 

 

I have been experimenting with the given model in the NX help tutorial for orbital radiation analysis, changed the orbit parameters input to a range that I am interested in. However, i realised that the results only gave temperature plots for increment 1, at 0sec and other increments does not show temperature results, only radiations. (I have attached a screenshot for reference)

troubleshoot.PNG

I would like to get a range of temperature plot as the satellite orbits the Earth though, to identify the maximum and minimum expected temperature for the satellite. Can i have any advice for how i can obtain this?

 

Thanks and have a nice day. Smiley Happy

Felchen 

2 REPLIES

Re: Orbital temperature range in space thermal system

Creator
Creator
Hi.

I think you need to select a Transient type of analysis

Re: Orbital temperature range in space thermal system

Experimenter
Experimenter

Hi

 

You Must Create Animation (With iteration)

 

Or

 

Create plot (With iteration)

 

And Select Time of (Or  Iteration)  To Show Maximum and Minimum   Temperature