Cancel
Showing results for 
Search instead for 
Did you mean: 

Pressure dialog box

Experimenter
Experimenter

I want to use distribution in the pressure dialog box in nx 10
How to active it in the dialog box iam working with sol 108 in the magnitude 2 i use table field

(pressure,frequency) i want to use distribution in the pressure dialog box 

it appears in nx 9 how to active it in nx 10 

2 REPLIES

Re: Pressure dialog box

Siemens Phenom Siemens Phenom
Siemens Phenom

It looks like you've already done this. Magnitude is set to Field. If the field named Magnitude(2) has an independent domain of Cartesian, then you have a spatial pressure distribution.

Re: Pressure dialog box

Experimenter
Experimenter
I Am working on a tutorial using sol108 in the magnitude i use a table (frequency ,pressure) i want do distribute the pressure on the model
In nx 9 and 8.5 the distribution is appears in the dialog box
How to use the distribution in nx 10