Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem in giving the angle of throttle valve in flow simulation

Experimenter
Experimenter

Hello all,

I am doing flow simulation in NX thermal/flow. I have a throttle vale inside a tube. The angle changes from 0 to 90 in steps of 10.. Is it correct to give it in flow surface as rotational parameters. It asks for the option of motion type and rotating rate.

 

I have give motion type as rotational and motion rate as 10 degree/sec. Is it correct or can any of you give suggestions on it. 

 

I have just attached the file. Unfortunately, it is in German.

 

Should I use any other options?

 

Ash