Cancel
Showing results for 
Search instead for 
Did you mean: 

Question regarding deselecting boundaries in fibersim

Experimenter
Experimenter

This should be real simple, but apparently it isnt. I want to deselect boundary curves one by one, not all at the same timeI am using NX 9 and Fibersim 14.

1. I create a boundary for a ply in fibersim
2. Click OK
3. Reenter the boundary editor to edit the boundary, but the orange boundary lines are unclickable. My only option is to deselect all.

Neither will the curve selector allow me to see the specific curves, only the amount of curves/lines chosen for the boundary. The picture shows the curve selector box not showing the selected curves.

I have tried shift + left click, alt + left click





2 REPLIES

Re: Question regarding deselecting boundaries in fibersim

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Markus

 

This is working for me with NX10 and Fibersim 14.1.

 

Have you tried changing the curve rule from 'connected curves' to 'single curve' and then SHIFT-left clicking?

 

Phil


Philippe Tremblay
phillippe.tremblay.ext@siemens.com
www.mayahtt.com

Re: Question regarding deselecting boundaries in fibersim

Experimenter
Experimenter

Hello,

I am using single-curve already. I can erase boundaries if I havent clicked OK and re-entered yet. I will try upgrading to NX10 and see if it gets any better...