Cancel
Showing results for 
Search instead for 
Did you mean: 

SOL 101 and SOL103 in single run

Experimenter
Experimenter

Is it possible to perform a modal analysis (SOL103) and a static computation  (SOL101) in a single run? The main goal is to recuperate the system matrices. Otherwise the mass and stiffnes matric are build twice.

 

Best Regards,

Karim

1 REPLY

Re: SOL 101 and SOL103 in single run

Siemens Phenom Siemens Phenom
Siemens Phenom

You can run SOL 103 with a static and a modal subcase. This is typically done for a pre-stressed modes analysis where the differential stiffness due to the static loading is included in the normal modes calculation. However, if the STATSUB case control in the normal modes case does not reference the static subcase, the modes will be unaffected and the static subcase and normal modes subcase results will be independent.