Cancel
Showing results for 
Search instead for 
Did you mean: 

Save options for SIM and FEM files

Phenom
Phenom
NX 5.0.4 TC 2005 SR1/2007

Our CAD users want "Save JT Data" and "Save Drawing CGM Data" on, in the Save Options.

Our CAE users want them off for the SIM and FEM files.

Is there a way to set the "Save Options" for specific file types?

Thanks,
Dave
-Dave
NX 11 | Teamcenter 11 | Windows 8.1
4 REPLIES

Re: Save options for SIM and FEM files

N/A
Different site level customer defaults?
Add a group level set of defaults for specific users?
This could be automated in start_ugmanager.bat if you can base it on whether (or not) NX/NASTRAN is installed...

But if the same user does CAD (where they want the JT/CGM) and CAE (where they don't) it probably won't work.

Re: Save options for SIM and FEM files

Phenom
Phenom
We have some users that do both, and sometimes they forget to toggle them off, or on, when needed. That's why I'd like to do it behind the scenes, if possible.

Thanks
-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: Save options for SIM and FEM files

Esteemed Contributor
Esteemed Contributor
See your second thread about this problem for an answer of mine.
Cross-posting ... ?
Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: Save options for SIM and FEM files

Phenom
Phenom
See your second thread about this problem for an answer of mine.

Cross-posting ... ?


Not sure if it was more of a CAD or an Analysis question...probably neither.

Thanks, saw your other reply.
-Dave
NX 11 | Teamcenter 11 | Windows 8.1