Cancel
Showing results for 
Search instead for 
Did you mean: 

Specifying the names of companion results in post processor

Valued Contributor
Valued Contributor

I have a simulation which produces a number of universal results files (.unv) from an in-house subroutine. I import these as companion results. However, they are all non-standard types such as mol fraction for which there is no option in the unv. At the moment I have imported them all as temperatures.

Is there a way I can rename them or have them take the name specified in the simulation navigator, rather than just "Data Type - Elemental/Nodal" ?

2 REPLIES

Re: Specifying the names of companion results in post processor

Siemens Phenom Siemens Phenom
Siemens Phenom

There are 3 keywords that you can define in the universal file dataset 2414 header to help customize the NX post processing Navigator and graphics window header:

 

  • LOADCASE_NAME_KEY
  • EXPRESSION_NAME_KEY
  • RESULT_NAME_KEY

 

These can be found in the online documentation under “Customizing universal dataset 2414”:

 

https://docs.plm.automation.siemens.com/tdoc/nx/10.0.2/nx_help/#uid:index_advanced:xid433696:id11265...

 

Re: Specifying the names of companion results in post processor

Valued Contributor
Valued Contributor
Thanks Jim! That's perfect.