Showing results for 
Search instead for 
Do you mean 
Reply

Surface wrap body - can it be manipulated in ideal or master part ?

In the fem part,  I have used the new 'surface wrap' capability to determine the inner volume of an acoustic enclosure. Is there any way to apply modeling techniques like boolean add,, etc, to be able to manipulate and tweak this polygon body in the ideal or the master part ? I guess the first step would be to somehow 'include' this polygon body into the ideal or master part. I thought I saw sometime ago a paper on how to push fem polygon bodies upstream to ideal/master part but cannot locate it now. Thanks.

 

Bulent

1 REPLY

Re: Surface wrap body - can it be manipulated in ideal or master part ?

You can create a sheet body in the master part from a polygon face in the FEM part. Note that the FEM must be displayed and the master part must be the work part for the command to be active.

 

See online help at:

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:index_advanced:xid389662:xid456876:x...

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:index_advanced:xid389662:xid456876