cancel
Showing results for 
Search instead for 
Did you mean: 

TEC / Peltier module and PID / regulation

Creator
Creator

Hello,

 

Even though I never used it, I know that it is possible to implement a controler for a heat charge. This permit to implement a regulation for a radiator.

 

Is it possible to do the same to simulate a regulation by a thermo electric module ?

 

Thanks

2 REPLIES

Re: TEC / Peltier module and PID / regulation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

 

All the parameters of the PELTIER Cooler module can have constant or Temperature dependent values, then you have a chance for controlling its value.

 

Also, in the Electrical Boundary Condition you can specify how the array is electrically connected:

 

  • If you choose Voltage, specify a constant, time dependent, or temperature dependent value for that voltage in Volts. The value may be positive or negative.
  • If you choose Current, specify a constant, time dependent, or temperature dependent value for current in Amps.

 

peltier.png

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: TEC / Peltier module and PID / regulation

Creator
Creator
Yes, I know that I can enter a temperature dependant value with the "field" option instead of "expression" entered by default. But how can I relate a temperature dependant law to the point of regulation of my system ? How can I choose which temperature is considered by this function ? Thanks