Cancel
Showing results for 
Search instead for 
Did you mean: 

Testing meshing ability of a polygon body in .part-file

Creator
Creator

Hi everybody,

 

is there a way to test the ability of mesh generation of an polygonbody when it is still a .part-file?

 

Thanks everybody.

 

Greetings

 

Werner

3 REPLIES

Re: Testing meshing ability of a polygon body in .part-file

Valued Contributor
Valued Contributor

If you're specifically looking for a way to test whether a 3D swept mesh could be applied to the body then use the Split Body command in NX Advanced Simulation. When using the Split Body command in Advanced Sim you have the option to Check for Sweepable Bodies and to automatically Create MMCs. Those options are not available when using the Split Body command in NX Modeling.

Re: Testing meshing ability of a polygon body in .part-file

Siemens Phenom Siemens Phenom
Siemens Phenom

Actually the check for sweepable bodies is available in Modeling as well, but it is fairly well hidden. Modeling development didn't want CAE use cases polluting their UI in general, so this option is buried in the Modeling Preferences. In Modeling, go to Menu, Preferences, Modeling, Simulation for one and only one toggle that controls the one and only one CAE specific UI widget in Modeling commands. That one command is Split Body and its check for sweepable bodies.

 

There are no other checks for meshable bodies in Modeling or CAE.

 

Regards,

Mark

 

 

Mark Lamping

Simulation Product Management

Simulation and Test Solutions

 

Siemens Industry Sector

Siemens Product Lifecycle Management Software Inc.

 

mark.lamping@siemens.com

www.siemens.com/plm

 

 

Re: Testing meshing ability of a polygon body in .part-file

Legend
Legend

What is this "polluting" you speak of, Marc?  You meant enhance, didn't you? Smiley Happy