Cancel
Showing results for 
Search instead for 
Did you mean: 

Thermal/Flow simulation with moving objects

Creator
Creator

Hello everyone!

Is it possible to simulate thermal and mass flows of the system with the moving objects?

I need to evaluate temperature and flow distribution in an elevator shaft. So I need to enter some data about how an elevator carriage are moving.

I cannot understand if it's possible with "Solid Motion Effects" of Simcenter Advanced Thermal/Flow.

1 REPLY

Re: Thermal/Flow simulation with moving objects

Legend
Legend

You should be able to use the moving frame of reference in NX/Flow.  It won't do any adaptive meshing or rigid body motion solve, but with will calculate the proper flow based on translation input