Cancel
Showing results for 
Search instead for 
Did you mean: 

Unclear warning in SOL601/106

Phenom
Phenom

Hi,

 

short question to all experts :

 

Why do I get the following warning when solving nonlinear solution 601-106 with ATS at the beginning in f06 file?

 

***WARNING: Large strain kinematic formulation is not applicable with material ** for PID **

 

I use MAT1, MATS1 and TABLES1 declaration and standard PSOLID parameter for parabolic Hexahedron eLements.

 

SOL 601,106
$* NX Modeling Object: ATS
NXSTRAT 100 AUTO 1 ATSSUBD 50
$* PARAM CARDS
PARAM ALPHA1 0.0000 0.0000
PARAM ALPHA2 0.0000 0.0000
PARAM LGSTRN 1
PARAM OMACHPR YES
PARAM POST -2
PARAM POSTEXT YES
PARAM UNITSYS MN-MM
$* PROPERTY CARDS
PSOLID 1 1 0 SMECH
$* MATERIAL CARDS
MAT1 11.1260+8 0.3000001.4000-6
MATS1 1 1 NLELAST 1 32.0000+5
TABLES1 1 +
+ -0.01000-2.050+5-0.00178-2.000+5 0.0000 0.00000.0017762.0000+5+
+ 0.0100002.0500+5 ENDT

 

Why do I get that warning?

Does my solution consider large strain assumptions? I do not know if this warning is realistic or not.

Does my definition parameters point out that my material declaration is not suitable for large strain kinematics?

 

As results I get nonlinear stresses and strains and therefore I believe solution is correct. But what does the warning mean?

 

Any suggestion will help. With best regards,

Michael

Production: NX10; Development: VB, TCL/TK, FORTRAN; Testing: NX11