Cancel
Showing results for 
Search instead for 
Did you mean: 

deactivate model setup check for solve all solution

Pioneer
Pioneer

Hi,

 

for a model with many solutions, I can solve all solutions in one action: "Solve All Solutions".

 

I make use of the "Advanced Solver Option" -> "Subset Export" in the "Export Options" tab, to work with a "Selected Group". For this process, NX requests the "Model Setup Check" to be de-activated.

 

But I can't find how to de-activate "Model Setup Check" for all solutions in the model when I launch a "Solve All Solutions", so there are errors which prevent the solving. I need to solve solutions one by one...Robot Mad

 

  • Could anybody tell me how to "globally" de-activate "Model Setup Check"?

 

thank you,

Cyril
4 REPLIES

Re: deactivate model setup check for solve all solution

Siemens Phenom Siemens Phenom
Siemens Phenom

Unfortunately, this cannot be done. The model check toggle is a property on the Solve dialog - it is not a property of the solution, so it cannot be set in advance.

 

The only workaround would be to write a custom "Solve All Solutions" journal to loop through all of the solutions and solve them. The API call to launch the solve for an individual solution (NXOpen.CAE.SimSolution.Solve()) takes the SetupCheckOption as its second argument so you could set it to "DoNotCheck" in the journal.

 

Fortunately, this journal is very simple:

 

VB:

Option Strict Off
Imports System
Imports NXOpen
Imports NXOpen.UF

Module SolveAllSolutions

    Sub Main()

        Dim theSession As Session = Session.GetSession()

        Dim SimPart As CAE.SimPart = theSession.Parts.BaseWork

        Dim Simulation As CAE.SimSimulation = SimPart.Simulation

        For Each solution As CAE.SimSolution In Simulation.Solutions

            Simulation.ActiveSolution = solution
            solution.Solve(CAE.SimSolution.SolveOption.Solve, CAE.SimSolution.SetupCheckOption.DoNotCheck)

        Next solution

    End Sub

End Module

  

Python:

import sys
import NXOpen
from NXOpen import CAE

theSession = NXOpen.Session.GetSession()

def main(*args): 

    SimPart = theSession.Parts.BaseWork

    Simulation = SimPart.Simulation

    for solution in Simulation.Solutions:

        Simulation.ActiveSolution = solution
        solution.Solve(CAE.SimSolution.SolveOption.Solve, CAE.SimSolution.SetupCheckOption.DoNotCheck)


# Main program.

if __name__ == "__main__":
    main()

 

 

Re: deactivate model setup check for solve all solution

Pioneer
Pioneer

Hello Jim,

 

thank you for your answer and helpfull advice, I will try the journal method as soon as I can.

 

Do you think if I file an ER the ability to choose "No Model Setup Check" could be an option in the NX Advanced Simulation Workflow of the "Solve All" command?

 

best regards,

Cyril

Re: deactivate model setup check for solve all solution

Pioneer
Pioneer

Hi Jim,

 

sorry for the latency, I only tried the vb today.

 

There seems to be an issue:

deactivate moel setup check

I have more solutions, some have already results.

 

Please let me know what information could be helpful.

 

yours sincerely,

Cyril

Re: deactivate model setup check for solve all solution

Siemens Phenom Siemens Phenom
Siemens Phenom

I updated the code in the original reply to include a line to set the solution as the active solution prior to solving.