Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

files for batch meshing

Hi all,

 

I have launch the batch meshing window, I have an error. Attached the log file error.

-------

"stdInput: ERROR: File not found
Appending d:\Users\Desktop\TESTS\ CAE BACTH MESHING\TEST MESH SOLID V1__FEM__MeshReport.LOG to d:\Users\Desktop\NX TESTS\CAE BACTH MESHING\LOG_140414174818.log"

-------

I am not sure, but I think that batch mesher needs 3 files, 1-ufx_batchmeshing_sample_criteria.txt, 2-ufx_batchmeshing_sample_param.txt and a

3-CAE .FEM template.

Actually, I have tried with both .TXT files with no succes on batch meshing.

Do I need the .FEM template too, with two .TXT files?

 

Thanks in advance,

2 REPLIES
Solution
Solution
Accepted by topic author Igor
‎08-26-2015 04:32 AM

Re: files for batch meshing

Igor, I think for someone to understand the problem, you need to actually attach the log file, but this may really a question for GTAC.
http://support.industrysoftware.automation.siemens.com/

Regards,

Ganesh

Regards,
Ganesh

Simcenter 3D Community Manager
Simulation and Test Solutions

Re: files for batch meshing

For the first steps I would recommend to use the batch mesher with the GUI. It can be started with the following command:

 

%UGII_ROOT_DIR%\launch_batchmesher.bat

 

All you have to do then is to select a CAD geometry and with defaults it should generate you a meshed part.