Cancel
Showing results for 
Search instead for 
Did you mean: 

memory access voilation while mapping temp from NX thermal to NX nastran

Pioneer
Pioneer
Hello Expert,

I followed the procedure given in NX 8.0 CAST to map the temperatures from NX thermal to NX nastran,

I could able to see while solving the mapping solution that mapping done successfully, while reading the temperatures in NX nastran, error message has popped up "memory access violation"

I use 64 bit OS, with 24GB RAM.

Please help me, Thanks in advance.

Thanks & Regards,
Dev.
1 REPLY

Re: memory access voilation while mapping temp from NX thermal to NX nastran

Innovator
Innovator
Dear Dev,
This error typicaly happens when you run NX AdvSim in a computer with 32 bits OS, not enough RAM memory available, but you say you runs a 64-bit OS, plenty of RAM with 24 GB, then this is not the reason.
Then I would suggest to check what version of both NX & NX THERMAL you have installed:
" Maintenance Pack 2 for NX 8.0.3 is now available.
" Thermal and Flow solver patch updates for NX are availale: 8.0.391 Nov 30, 2012
Check what versions you have installed, and update your software if necessary.
Best regards,
Blas.