Cancel
Showing results for 
Search instead for 
Did you mean: 

tire/wheel/rolling contact modeling in NX/Motion

Has anyone been successful modeling rolling contact in NX/Motion without significant numerical chatter? Are there examples anywhere? The attached pdf shows a very simple model of a "car" with 4 wheels. Changes to contact settings, friction, etc does not seem to settle the noise down. Force in the x-direction in the plot shown should be zero (constant). 

 

Thank You,

 

Chris Muir

1 REPLY

Re: tire/wheel/rolling contact modeling in NX/Motion

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi,

 

At first glimpse, I would suggest to change the sphere geometry into cylinder instead, because the cylinder geometry has more geometry to possibly in-contact with the flat ground, thus help to reduce noise. 

 

Furthermore, I think you can try to play around with the damping values in the 3D contact definition, which might help in your case.

 

Kind regards,

Tuw