Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Cant start NX 9

Experimenter
Experimenter

Hi,

I installed NX9 to use it on my MacBook. But I cant start it. I have the student edition.

It opens X11 and shows the loading screen but than it closes.

 

I think there are two possible reasons for the problem.

- I updated my Mac to Mac OS Yosemite. Does NX allready work with Yosemite?

- The licensing tool shows the Mac-adress of my WLAN-router but in my license file is my personal MAC adress registererd. Do I need a wired connection to start NX?

 

H3NK

 

 

2 REPLIES

Re: Cant start NX 9

Experimenter
Experimenter

NX9 is not supported on Mac OS 10.10...

 

Can I get a student Version of NX 10? Or do I have to downgrade to Mac OS 10.9?

Re: Cant start NX 9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is no need for a wired LAN connection, but the network adapter you registered NX with needs to be enabled.

 

BTW, this forum is for questions about the forum only, for student editions it is best to ask in the academic forum.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide