Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Spring at Non linear

Experimenter
Experimenter

Dears.

 

I have a simple question, which its diggin my head.

Supposed to have a single two nodes separeted 100mm in X direcction, where the I do link a CBUSH spring in betwen, in one side of the spring it's fixed the node as 123, however in another side I place a linear desplacement which is variable by the time, on which at stage 1 goes to the desplacement needed, but at the stage two the side of the spring is loosed/released i.e. (considering the retribucion/bouncing as a negative diplacement when the side of the spring is stretched and then loosed without appling any load, just displacement at the stage 1)

Is that possible?

 

 

Thanks and regards.