Cancel
Showing results for 
Search instead for 
Did you mean: 

API - Delete elements lying within an enclosed curve

Valued Contributor
Valued Contributor

Hi, Is there a direct way to delete the elements lying within a closed curve. The elements and curves lie on the same plane. I can only think of getting the coordinates of the points of the curves, and then compare it with the CG coords of elements and delete which lies within the vertices of closed curve. This process could be time consuming. Are there any other tricks?

 

Thank you

Kannan

2 REPLIES 2

Re: API - Delete elements lying within an enclosed curve

Siemens Phenom Siemens Phenom
Siemens Phenom

Give this a try, it might be a way to get what you're looking for. 

 

The API will prompt you to select a surface and then select your curves that make up your boundary. Those curves will be projected into the surface creating two different surfaces. It will then remesh the original surface using the attributes, leaving the new surface without mesh.


The HTML Clipboard

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim crvSet As femap.Set
    Set crvSet = App.feSet

    Dim srfSet As femap.Set
    Set srfSet = App.feSet

    Dim dSet As femap.Set
    Set dSet = App.feSet

    Dim eSet As femap.Set
    Set eSet = App.feSet

    Dim sID As Long

    If srfSet.SelectID(FT_SURFACE, "Select Surface to Project Onto", sID) <> FE_OK Then End

    If crvSet.Select(FT_CURVE, True, "Select Curves as Bounds") <> FE_OK Then End

    App.feCurveProjectCurvesOntoSurfaces(crvSet.ID, srfSet.ID, 0, True)

    rc = App.feMeshSurface2(-sID, 0, 0, False, False)

    App.feViewRegenerate(0)

End Sub

Re: API - Delete elements lying within an enclosed curve

Valued Contributor
Valued Contributor

Thats a good idea. Thanks.