Cancel
Showing results for 
Search instead for 
Did you mean: 

API Extract Nodal Stresses from Element Stresses in Output Vector

Creator
Creator

Hello all,

 

I am looking to programmatically extract the nodal stress data at every node. I know the output set I am looking for as well as the output vector.

'Get model
Dim App As femap.model
Set App = feFemap()

'Output Set object
Dim curOutputSet As femap.OutputSet
Set curOutputSet = App.feOutputSet
'Output Vector object
Dim curOutputVect As femap.Output
Set curOutputVect = App.feOutput

Dim theOutputSetID As Long
theOutputSetID = 16
Dim theOutputVectID As Long
theOutputVectID = 60031

'Get output set and output vector
curOutputSet.Get(theOutputSetID) curOutputVect.GetFromSet(curOutputSet.ID, theOutputVectorID)

The data received inside curOutputVect is for the elements. I can see that curOutputVect.values has the elemental stresses at the indices matching the Element IDs and that there are object methods like GetOutputListAtSet() that can get the same data.  However, I would like to extract the averaged nodal stresses for the nodes of these elements, and unless I am missing something obvious, they don’t seem to be available through this object. I can get to these values with the GUI into the Data Table using these steps:

 View->Select…->Deformed and Contour Data…

Select Contour Options…

In Contour Type, select “Nodal” radio button

In Data Conversion, select “Average”

(Make sure Data Table is open and unlocked)

 Now List->Output->Contoured Results to Data Table… will write out the values to the Data Table:dataTable.png

Is there a way I can get these values through the API, or replicate the process above programmatically and extract directly from the generated Data Table?

Regards,

Ryan

4 REPLIES 4

Re: API Extract Nodal Stresses from Element Stresses in Output Vector

Siemens Phenom Siemens Phenom
Siemens Phenom

The API output object does not support conversin between nodal and elemental locations. There are however at least two ways to accomplish this. You can use the application level feOutputProcessConvert( ) method to create new vectors at the desired location (see API manual 3.8.3.6). Or, you can use the Results Browsing object and use the AddConversionColumn( ) method (see API manual 4.9.7.3). For general querying of results I would recommend using the Results Browing object. If you need to do additional computations feOutputProcessConvert( ) might be more appropriate

Re: API Extract Nodal Stresses from Element Stresses in Output Vector

Creator
Creator

This is exactly what I am looking for! Thank you so much.

 

I went with the Results Browsing object.

 

Resulting code (for future interest of thread):

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim getNodalData As femap.Results
    Set getNodalData = App.feResults

    Dim currentView As femap.View
    Set currentView = App.feView

    Dim curOutputSet As femap.OutputSet
    Set curOutputSet = App.feOutputSet

    Dim curOutputVect As femap.Output
    Set curOutputVect = App.feOutput

    Dim grpAllNodes As femap.Group
    Set grpAllNodes = App.feGroup

    Dim allElems As femap.Set
    Set allElems = App.feSet

    Dim allNodes As femap.Set
    Set allNodes = App.feSet

    Dim columnIndex As Long
    Dim nIDsArr As Variant
    Dim nValsArr As Variant
    Dim numCols As Long

    Dim activeViewID As Long

    Dim rc As femap.zReturnCode

    'get a group of elements from the user for getting node stress data
    rc = grpAllNodes.SelectID("Select group of elements for node stresses")
    If Not (rc = femap.zReturnCode.FE_OK) Then
        Exit Sub
    End If

    'get current view (to define the output set and output vector)
    App.feAppGetActiveView(activeViewID)
    currentView.Get(activeViewID)

    'get elements from group
    allElems.AddGroup(FT_ELEM, grpAllNodes.ID)
    'get nodes from elements
    allNodes.AddSetRule(allElems.ID, FGD_NODE_ONELEM)

    'get current output set
    curOutputSet.Get(currentView.OutputSet)

    'Get current output vector
    curOutputVect.GetFromSet(curOutputSet.ID, currentView.ContourData)

    'consider only the elements in a particular group
    rc = getNodalData.DataNeeded(FT_ELEM, allElems.ID)
    'convert to nodal stress
    rc = getNodalData.AddConversionColumn(curOutputSet.ID, curOutputVect.ID, femap.zResultsConvert.FRC_AVG, columnIndex )
    'populate this column with data
    rc = getNodalData.Populate()
    'get data from the column populated
    rc = getNodalData.GetColumn(columnIndex, nIDsArr, nValsArr)

    'Now nValsArr holds the data
    
End Sub

Re: API Extract Nodal Stresses from Element Stresses in Output Vector

Hi Ryan,

 

thanks for that code, I need nodal stress outside of FEMAP as well.

 

Since I have poor experience in FEMAP:

 

- How do I get the stresses (nValsArr) out now? for example into the data table or, even better into a *.csv file?

 

thanks,

 

der Rechenschieber

Highlighted

Re: API Extract Nodal Stresses from Element Stresses in Output Vector

Siemens Phenom Siemens Phenom
Siemens Phenom

Sending to Data Table and saving the CSV is appended at the bottom.  You could also write and open data directly to Excel. I can give you an example if that is your ultimate goal.

 

The HTML Clipboard

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim getNodalData As femap.Results
    Set getNodalData = App.feResults

    Dim currentView As femap.View
    Set currentView = App.feView

    Dim curOutputSet As femap.OutputSet
    Set curOutputSet = App.feOutputSet

    Dim curOutputVect As femap.Output
    Set curOutputVect = App.feOutput

    Dim grpAllNodes As femap.Group
    Set grpAllNodes = App.feGroup

    Dim allElems As femap.Set
    Set allElems = App.feSet

    Dim allNodes As femap.Set
    Set allNodes = App.feSet

    Dim columnIndex As Long
    Dim nIDsArr As Variant
    Dim nValsArr As Variant
    Dim numCols As Long

    Dim activeViewID As Long

    Dim rc As femap.zReturnCode

    'get a group of elements from the user for getting node stress data
    rc = grpAllNodes.SelectID("Select group of elements for node stresses")
    If Not (rc = femap.zReturnCode.FE_OK) Then
        Exit Sub
    End If

    'get current view (to define the output set and output vector)
    App.feAppGetActiveView(activeViewID)
    currentView.Get(activeViewID)

    'get elements from group
    allElems.AddGroup(FT_ELEM, grpAllNodes.ID)
    'get nodes from elements
    allNodes.AddSetRule(allElems.ID, FGD_NODE_ONELEM)

    'get current output set
    curOutputSet.Get(currentView.OutputSet)

    'Get current output vector
    curOutputVect.GetFromSet(curOutputSet.ID, currentView.ContourData)

    'consider only the elements in a particular group
    rc = getNodalData.DataNeeded(FT_ELEM, allElems.ID)
    'convert to nodal stress
    rc = getNodalData.AddConversionColumn(curOutputSet.ID, curOutputVect.ID, femap.zResultsConvert.FRC_AVG, columnIndex )
    'populate this column with data
    rc = getNodalData.Populate()
    'get data from the column populated
    rc = getNodalData.GetColumn(columnIndex, nIDsArr, nValsArr)

    'Now nValsArr holds the data

    Dim dTable As DataTable
    Set dTable = App.feDataTable

    App.feAppManagePanes("Data Table",1) 'Make Data Table Visible
    dTable.Lock(False) ' Unlock Data Table

    getNodalData.SendToDataTable() 'Send Results Browsing values to Data Table

    Dim fName As String
    If App.feFileGetName ("Export Data to CSV", "Comma Seperated File", "*.csv",True,fName) <> FE_OK Then End

    dTable.Save(True, fName, FSF_CSV)

End Sub