Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

API for surface set offset

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Hi all, to offset 1 Surface I use rc = App.feSurfaceOffset(surfID,0.1) I can not find a similar command to offset a surface set (more than 1 surface in a single command without looping over surfID) Thank you
2 REPLIES 2

Re: API for surface set offset

Phenom
Phenom

It doesn't look like there is a set equivalent of feSurfaceOffset, but perhaps feSurfaceOffsetTangent will be useful, if the starting surface is recursively tangent to multiple others which you wish to offset in a single command.

Otherwise it looks like a loop over the surfaces in your set will be required.

Re: API for surface set offset

Siemens Phenom Siemens Phenom
Siemens Phenom

We have added feSurfaceOffset2 for FEMAP v12, where one can specify a Set ID containing multiple FEMAP surfaces for offset.

 

Mark.