Cancel
Showing results for 
Search instead for 
Did you mean: 

API to read a TEXT file into femap

Pioneer
Pioneer

I am trying to use a TEXT File to read in data into femap, but I am having some difficulty in getting the code right.

Below I have the code and attatched the .txt file.

 

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim readFile As femap.Read
    Set readFile = App.feRead

    Dim s As femap.Surface
    Set s = App.feSurface

    Dim colorSet1 As femap.Set, colorSet2 As femap.Set
    Set colorSet1 = App.feSet
    Set colorSet2 = App.feSet

    Dim sSet As femap.Set, gr As femap.Group
    Set sSet = App.feSet

    Dim thickness As Variant
    Set gr = App.feGroup

    Dim t As String

    rc = App.feFileGetName( "Select File with FemapColorID", "Text Files", ".txt", True, t)
    If rc = FE_OK Then
        rc = readFile.Open(t, 80)
        If rc = FE_OK Then
            While Not readFile.AtEOF
                rc = readFile.Read
                gr.ID = readFile.RealField (1,0)
                colorSet2.ID = readFile.IntField (2, 0)
                thickness = readFile.IntField (3,0)
            Wend
    End If
        End If


    While s.Next
        If colorSet1.IsAdded(s.color) = FE_FAIL Then
            colorSet1.Add(s.color)
            colorSet2.Add(s.ID)
        End If
    Wend

    While colorSet2.Next
        sSet.Clear


        sSet.AddRule(colorSet2.CurrentID,FGD_SURFACE_BYCOLOR)
        gr.SetAdd(FT_SURFACE,sSet.ID)

       s.Get(colorSet2.CurrentID)
           gr.title = "Plate =  " & thickness
        gr.Put(gr.ID)

    Wend

End Sub
 

 

Basically I want to bring in a model into femap whereby the model is different colors based on its thickness. So I would like femap to read in the text file and then create groups based on the color of the surfaces.

 

Thanking you in advance

4 REPLIES 4

Re: API to read a TEXT file into femap

Phenom
Phenom

Hi RedP,

 

A few tips & questions:

 

1) add the star in the getfilename method: "*.txt"

 

2) is there a specific reason for the group IDs to appear? Or is it enough if the macro creates a group without over writing any already existing group? if the later you can delete the "groupID" column and use gr.put(gr.NextEmptyID).

This is a general comment: FEMAP is very good in dealing with IDs. Unless you have a precise reason for forcing IDs, leave this consideration to FEMAP.

 

3) now the tricky, convoluted part: from what I understand you want a corrspondance between color and thickness (indicated in group title). This can't be done thourgh a set, because the order will be lost. This needs to be done in an array or a dictionnary (better), i.e. something like a table which stores face to face a color number and a thickness.

 

You've reused the bit of code I gave you earlier, but I don't think that's the right idea. There is a trick to understand what the code does, with the SURFACE_BY_COLOR rule.

When you write set1.addRule(myID, FGD_SURFACE_BY_COLOR), myID DOES NOT refer to a color, it refers to a surface. So the command means "I want you to fill set1 with all surfaces which have the same color as surface #myID."
This is not really intuitive and a bit tricky (or so I think) in the FEMAP API world, because usually the ID directly refers to what we point to. For ex with ELEM_BYPROP, you give the ID of a prop, not an element using a prop. But anyway...

 

 

Here's how I would solve your problem (NB: there are many ways to do this):

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim t As String

    Dim readFile As femap.Read
    Set readFile = App.feRead

    Dim s As femap.Surface
    Set s = App.feSurface

    Dim gr As femap.Group
    Set gr = App.feGroup

    Dim colorSet As femap.Set, sSet As femap.Set
    Set colorSet = App.feSet
    Set sSet = App.feSet

    Dim thickDict As Object
    Set thickDict = CreateObject("Scripting.Dictionary")

    '1) Read file
    If App.feFileGetName("Select File with FemapColorID","Text Files","*.txt",True,t) _
        = FE_CANCEL Then End
    readFile.SetNoBlankLines(True)
    readFile.Open(t, 80)

    'skip 2 lines
    readFile.Read : readFile.Read

    While Not readFile.AtEOF
        readFile.Read
        colorSet.Add(readFile.IntField(1,0))
        thickDict.Add(readFile.IntField(1,0),readFile.IntField(2,0))
    Wend
    readFile.Close

    '2) Create groups per color and name them
    While s.Next
        If colorSet.IsAdded(s.color) Then
            Set gr = App.feGroup
            sSet.Clear
            sSet.AddRule(s.ID,FGD_SURFACE_BYCOLOR)

            gr.SetAdd(FT_SURFACE,sSet.ID)
            gr.title = "Plate Thickness " & CStr(thickDict.item(s.color))
            gr.Put(gr.NextEmptyID)

            colorSet.Remove(s.color)
            If colorSet.Count = 0 Then End
        End If
    Wend
End Sub

Re: API to read a TEXT file into femap

Phenom
Phenom

NB: this works for a text file in which there are only 2 columns: color ID ans plate thickness.

 

A little explanation as to why I've coded this like this: because of the trick "anomaly" I"ve explained on the the SURFACE BY COLOR rule, I can't loop on colors: I need to loop on surfaces. But I only want to loop once on surfaces: as a rule a thumb keep in mind that a good code should loop as little as possible.

So i'm going to loop on surfaces (i.e. on surface IDs), which means I have no clue as to in which order I will encouter surfaces which have a color you are interested in. So I need to the plate thicknedd correspondance in an object which is robust with regard to this "no specific order" concept: that is exactly what the dictionnary does.

 

The before-last line makes sure that once I've dealt with a color I dont deal with it again.

The last line simply exits once we're done with all colors.

 

Because of the tricky bit this whole subject treads on advance programming considerations: code complexity and optimization and code robustness with regard to user input. For ex I have not asked you whether your text file lists ALL possible colors in model, or whether it is possible that a color appears in the text file but does not in the model - as the code is written it is robust to all that.

 

AP

Re: API to read a TEXT file into femap

Pioneer
Pioneer

@astrium_tls

 

To answer your questions :

 

Yes there is a specific reason the group IDs appear cause i would like to seperate the sarface of color groups away from the others so that is why the group IDs appear so that then I wouldn't have to renumber is manually and the surfaces are grouped sequentially in an ascending order. And yes the text file does list all possible colors in the model. 

 

I really appreciate all the help and the explanations make a big difference thanks a lot, although I just have one last question, when I ran the code the first two thickness in the textfile the thickness 2 which is correspondent to color ID 122 and thickness 4 which is correspondent to color ID 119, it did not group these two colors, why would that be ???

 

Thanks again.

Re: API to read a TEXT file into femap

Pioneer
Pioneer

@astrium_tls

 

I've now realised why its skips the first two, in the code its skips two lines and then I altered my text file a bit. Thanks.