Can Femap display NX Nastran solid laminate material orientations?

Experimenter
Experimenter

For NX Nastran the material orientation for solid laminates uses the CORDM and the PSDIR field to select the closest element axis to use for the Z direction. Femap only displays the material orientation using exactly the direction from the coordinate system instead of using the closest element axis. Is there a way to visualise the actual NX Nastran material orientation for solid laminate elements in Femap?