Cancel
Showing results for 
Search instead for 
Did you mean: 

Can anyone run example 31? (Is SOL 601/701 available in the trial?)

Not applicable
Hey everyone.

I don't seem to be able to run any of the advanced nonlinear analysis modules (Advanced Nonlinear Static/Transient/Explicit).

When I run these modules they fail right after translation, and when I load the results and look at the 'user information message' I see the error 'Could not check out NX Nastran Advanced Nonlinear licence feature'.

Does the trial licence just not cover SOL 601/701? Anyone who doesn't know the answer to this, can you run example 31 from the help menu?

Any information would be helpful.

Thank you
Matthew
2 REPLIES

Re: Can anyone run example 31? (Is SOL 601/701 available in the trial?)

Not applicable
Found the answer if anyone's curious; no the trial licence doesn't cover it, but it can be enabled for the trial if you call the Global technical access center.

Re: Can anyone run example 31? (Is SOL 601/701 available in the trial?)

Creator
Creator

I'm finding GTAC Service too slow from my side despite calls & emails.