Highlighted

Change Membrane to Plate Elements

Pioneer
Pioneer

HI

I am having a properties say with membrane elements, can I change to Plate elements from Membrame elements.

 

I tried to the following Options, but it is not getting Update

 

Modify->Update Elements->Type

Modify->Update Elements->Formulation

 

Regards

srini

 

5 REPLIES 5

Re: Change Membrane to Plate Elements

Genius
Genius

Modify...

Update elements...

Type...

select all the elements you want to change... then OK

a window will appear and choose the new property (see picture) then press OK

 

Best Regards

 

AMinati

Re: Change Membrane to Plate Elements

Pioneer
Pioneer

I am observing existing Property tables instead of standard element type library

Error.png

Re: Change Membrane to Plate Elements

Siemens Phenom Siemens Phenom
Siemens Phenom

If you don't have any plate properties in your model, you must create a new plate property before hand or create a new one by selecting the button off to the right.  
Create property.png
Then select "Elem/Property Type" to change the type.
Elem type.png
Then select "Plate" as your type.
plate type.png
You can now fill out the info of the new plate property.
Plate prop info.png

Re: Change Membrane to Plate Elements

Genius
Genius

I don't know if you can create a new property when you modify a property. I am sure that if exist other properties you can change the elements property to the new one.

 

I have see the previous post, you can create a new as suggested

 

Best regards

AMinati

Re: Change Membrane to Plate Elements

Pioneer
Pioneer

Thank you so much Folks. I am assuming there will be an option to change from Membrane element without creating the property to the Plate elements. Other Pre-Processor do have this option